Lenses
(for Machine Vision) Vision System Peripheral Equipment CA-L Series

Lens Filters/OptionsLens filters support a variety of image detection needs.
CA-LF

Sharp cut filter (R60)
Sharp cut filters only allow light of a wavelength longer than a certain wavelength limit to pass.
Using these filters in combination with red LED lights makes it possible to capture images in which the ambient light is suppressed.

Without sharp cut filter
The fluorescent light is reflected by the metal surface.

With sharp cut filter
Ambient light is suppressed, which enables stable imaging.

Without sharp cut filter
The fluorescent light is refracted inside of the bottle, which makes inspections of the bottle opening difficult.

With sharp cut filter
The influence of the fluorescent light can be reduced.

Polarizing filter
Light (1) is polarized with polarizing filter A so only horizontal light (2) is transmitted to the target. Because polarizing filter B is set to accept vertical light only, the specular light (3) reflected from the film surface is rejected. However, the diffuse reflected light (4) from the target has a vertical component (5) that is allowed to pass through B to the camera.

Without polarizing filter
There is an imprint of the ring light.

With polarizing filter
The light imprint is reduced.

Protective filter
- The protective filter ensures a long service life of the lens by preventing damage during lens maintenance.
- During lens maintenance, all that needs to be done is replace the protective filter, which can be washed with water.
- The protective filter protects the lens surface from damage caused by processed chips.
- The protective filter eliminates the time and effort that is required to perform maintenance on the lens when oil mist or dust affixes to its surface.

Blue cut filter
The blue cut filter blocks the wavelength of blue LED light. Use this filter in combination with the wavelength conversion sheet to cut the excess blue LED light components that shine on the workpiece.