LED Lighting Vision System Peripheral Equipment CA-D Series

Line Lights High-intensity LED lights designed for use with line scan cameras
CA-DZWx

Line scan camera application examples
Area scan camera
Processing is performed by capturing the entire 2D image area at once, so it is not possible to obtain an optimal image due to the influence of the curved parts.

Line scan camera
Processing is performed on an image that is developed by capturing one pixel line at a time as the part is rotated. An optimal image is obtained since the capture condition is the same for each line, there is no halation effect from the curved parts.