Speed Control Based on Winding Amount
- CASE
- Steel
Ensure stable processing speed by adjusting the feeding speed according to the winding amount of the steel sheet.

Connect to IoT
Continuous processing line of steel sheets requires optimization of the processing speed in the entire facility.
Processing data on the same platform as the other equipment allows easy optimization of the entire facility.
Related productIL Series
The following data can be obtained.
Process data | Winding amount, judgment output (High, Low, Go), and alarm output |
---|---|
Diagnosis service data | Self-diagnosis status of the measurement system (errors, etc.) |