Steel Sheet Width Management During Rolling
- CASE
- Steel
Continuously check that the steel sheet width is within tolerance and record the result.

Connect to IoT
Centralized management including other data such as X-ray thickness measurement, profile measurement, and defect detection allows easy process improvement of the entire rolling process.
When an error occurs in a measurement system, it is indicated in real time so downtime can be minimized.
Related productIG Series
The following data can be obtained.
Process data | Target width, judgment output, alarm output, and control signal |
---|---|
Diagnosis service data | Self-diagnosis status of the measurement system (errors, etc.) |