Managing the Roll Chucking Position of a Slitter
- CASE
- Steel
Check the chucking position of a slitter stand or rough leveler roll.

Connect to IoT
The judgment threshold, which varies depending on the type of slitter, is automatically sent from the PLC.
The position is adjusted accordingly so the operators do not need to know any detailed information.
Related productIL Series
The following data can be obtained.
Process data | Chucking position, judgment output (High, Low, Go), alarm output, and control signal |
---|---|
Diagnosis service data | Self-diagnosis status of the measurement system (errors, etc.) |