Checking the Gap Between Rollers
- CASE
- Steel
Continuously measure the gap between the work rollers, which determines the plate thickness accuracy and flatness. These values can be displayed in the central control room for recording.

Connect to IoT
The continuous monitoring of numerical data allows countermeasures against errors to be taken in real time to minimize downtime.
Related productIG Series
The following data can be obtained.
Process data | Gap between work rollers, judgment output, alarm output, and control signal |
---|---|
Diagnosis service data | Self-diagnosis status of the measurement system (errors, etc.) |