Temperature Management During Film Stretching
- CASE
- Resin/Plastic Molding
Temperature affects the quality (molecular orientation) of the film, when the film is being stretched. Record the processing temperature in case there are problems after the product is sold.

Connect to IoT
Records of the processing temperature increases customers' confidence.
Batch management of the data on the same platform as the related information including date/time, product type, and roller rotation speed is useful for not only traceability but also quality improvement.
Related productFT Series
The following data can be obtained.
Process data | Temperature and judgment output (High, Low, Go) |
---|