Static Electricity Elimination in a Cell Production Process
- CASE
- Resin/Plastic Molding
Eliminate static electricity during assembly and record the result on the server.

Connect to IoT
If static electricity is often suspected as the cause of defects, recording data is a quick way to dispel doubt and solve the problem.
Related productSK Series
The following data can be obtained.
Process data | Static electricity level, temperature, humidity, judgment output (High, Low, Go), and alarm output |
---|---|
Diagnosis service data | Self-diagnosis status of the measurement system (errors, etc.) |