International System of Units (SI)

The principle behind the International System of Units is to provide the same values for measurements such as length, weight, and time no matter where in the world measurement is performed. The units used in this system are referred to as “SI units.” The system was established at the 1960 General Conferences on Weights and Measures (CGPM). The abbreviation “SI” stands for “Le Système International d'Unités.”

The International System of Units comprises the following three categories.

Base Units

Amount Unit name Unit symbol Definition
Length
Unit name
Meter
Unit symbol
m
Definition
The distance traveled by light in a vacuum in 1/299792458 second.
Weight
Unit name
Kilogram
Unit symbol
kg
Definition
This is the unit for weight. The mass of the international prototype kilogram.
Time
Unit name
Second
Unit symbol
s
Definition
The duration of 9192631770 periods of the radiation corresponding to the transition between the two hyperfine levels of the ground state of the cesium 133 atom.
Current
Unit name
Ampere
Unit symbol
A
Definition
The constant current which, if maintained in two straight parallel conductors of infinite length, of negligible circular cross-section, and placed 1 m apart in vacuum, would produce between these conductors a force equal to 2×10-7 newtons per meter of length.
Thermodynamic temperature
Unit name
Kelvin
Unit symbol
K
Definition
1/273.16 of the thermodynamic temperature of the triple point of water.
Substance amount
Unit name
Mole
Unit symbol
mol
Definition
The amount of substance of a system that contains as many elementary entities as there are atoms in 0.012 kilogram of carbon 12. (Limited to objects with clarified composition.) Elementary entities are subatomic particles that compose matter and energy.
Luminosity
Unit name
Candela
Unit symbol
cd
Definition
The luminous intensity, in a given direction, of a source that emits monochromatic radiation of frequency 540×1012 hertz and that has a radiant intensity in that direction of 1/683 watt per steradian.

Supplementary Units

Amount Unit name Unit symbol Definition
Plane angle
Unit name
Radian
Unit symbol
rad
Definition
Radian describes the plane angle subtended by an arc of a circle with the same length as the radius of that circle corresponds to an angle of 1 radian.
Solid angle
Unit name
Steradian
Unit symbol
sr
Definition
A steradian is a solid angle at the center of a sphere subtending a section on the surface equal in area to the square of the radius of the sphere.

We’re here to provide you with more details.
Reach out today!

Ask an Expert

Derived Units

Derived units are a combination of base units and supplementary units and the mathematical symbols of multiplication and division.

Amount Unit name Unit symbol
Area
Unit name
Square meter
Unit symbol
m2
Volume
Unit name
Cubic meter
Unit symbol
m3
Speed
Unit name
Meter per second
Unit symbol
m/s
Acceleration
Unit name
Meter per second squared
Unit symbol
m/s2
Wavenumber
Unit name
Reciprocal meter
Unit symbol
m-1
Density
Unit name
Kilogram per cubic meter
Unit symbol
kg/m3
Current density
Unit name
Ampere per square meter
Unit symbol
A/m2
Magnetic field strength
Unit name
Ampere per meter
Unit symbol
A/m
Concentration (of amount of substance)
Unit name
Mole per cubic meter
Unit symbol
mol/m3
Specific volume
Unit name
Cubic meter per kilogram
Unit symbol
m3/kg
Luminance
Unit name
Candela per square meter
Unit symbol
cd/m2

Some derived units are given unique names.

Amount Unit name Unit symbol Composition
Frequency
Unit name
Hertz
Unit symbol
Hz
Composition
1Hz=1s-1
Force
Unit name
Newton
Unit symbol
N
Composition
1N=1kg・m/s2
Pressure, stress
Unit name
Pascal
Unit symbol
Pa
Composition
1Pa=1N/m2
Energy, work, amount of heat
Unit name
Joule
Unit symbol
J
Composition
1J=1N・m
Power, radiant flux
Unit name
Watt
Unit symbol
W
Composition
W=1J/s
Electric charge, amount of electricity
Unit name
Coulomb
Unit symbol
C
Composition
1C=1A・s
Electric potential/electric potential difference, voltage, electromotive force
Unit name
Volt
Unit symbol
V
Composition
1V=1J/C
Resistance (electrical)
Unit name
Ohm
Unit symbol
Ω
Composition
1Ω=1V/A
Conductance (electrical)
Unit name
Siemens
Unit symbol
S
Composition
1S=1Ω-1
Magnetic
Unit name
Weber
Unit symbol
Wb
Composition
1Wb=1V・s
Magnetic flux density, magnetic induction
Unit name
Tesla
Unit symbol
T
Composition
1T=1Wb/m2
Inductance
Unit name
Henry
Unit symbol
H
Composition
1H=1Wb/A
Celsius temperature
Unit name
Degree Celsius
Unit symbol
°C
Composition
1t=T-To
Luminous flux
Unit name
Lumen
Unit symbol
lm
Composition
1lm=1cd・sr
Illuminance
Unit name
Lux
Unit symbol
lx
Composition
1lx=1lm/m2

Discover more about this product.
Click here to book your demo.

Experience Demo / Test

Reference Information

SI unit prefixes indicating integer powers of ten

Factor Prefix Symbol Factor Prefix Symbol
1018
Prefix
exa
Symbol
E
10-1
Prefix
deci
Symbol
d
1015
Prefix
peta
Symbol
P
10-2
Prefix
centi
Symbol
c
1012
Prefix
tera
Symbol
T
10-3
Prefix
milli
Symbol
m
109
Prefix
giga
Symbol
G
10-6
Prefix
micro
Symbol
µ
106
Prefix
mega
Symbol
M
10-9
Prefix
nano
Symbol
n
103
Prefix
kilo
Symbol
k
10-12
Prefix
pico
Symbol
p
102
Prefix
hecto
Symbol
h
10-15
Prefix
femto
Symbol
f
10
Prefix
deka
Symbol
da
10-18
Prefix
atto
Symbol
a

Non-SI units

Amount Unit name Unit symbol Definition
Time
Unit name
Minute
Unit symbol
min
Definition
1min=60s
Unit name
Hour
Unit symbol
h
Definition
1h=60min
Unit name
Day
Unit symbol
d
Definition
1d=24h
Plane angle
Unit name
Degree
Unit symbol
°
Definition
1°= (π/180) rad
Unit name
Minute
Unit symbol
Definition
1′= (1/60) °
Unit name
Second
Unit symbol
Definition
1″= (1/60) ′
Volume
Unit name
Liter
Unit symbol
l, L
Definition
1l=1dm3
Weight
Unit name
Metric ton
Unit symbol
t
Definition
1t=103kg

Evolution of SI Measurement Systems

The formation of the International System of Units, known as SI from the French Systeme International s’Unites, is the result of an international calibration towards a standardized system of measurements. The First Industrial Revolution brought about the rise of the textile industry and significant developments in metallurgy and coal mining.

However, most regions of the world relied on local units and standards that varied significantly from one place to another. Thus, the French introduced the SI measurement system as a revolutionary idea aimed at creating a uniform and logical system of measurement to appease the growing complexities of science, engineering, and trade, all of which demanded standardization.

The SI system went through several iterations between the 18th century and the 1960s before it was formally established during the 11th General Conference on Weights and Measures. This particular event defined the SI based on the physical constants of nature (seen in the table above) instead of tangible objects, thus ensuring greater precision and universality when using distance sensors.

We’re here to provide you with more details.
Reach out today!

Ask an Expert

Real-World Applications of SI Units

Since it provides universal and standardized measurements, the international unit system is widely used in modern industries and research and development settings. It enables effective communication between virtually everyone involved in the manufacturing of scientific processes.

Here are some key areas in which the SI system is used:

Engineering and Construction

Precision is the foundation of safety, efficiency, and innovation in engineering and construction, and the introduction of the international unit system enabled engineers worldwide to share and apply knowledge seamlessly. For example, architects rely on meters and kilograms to calculate structural integrity, while electrical engineers and technicians rely on amperes to design adequate and safe electrical systems.

Science and Research

The international unit system is the universal language of science since it enables researchers and scientists (and everyone else involved in manufacturing and R&D) to share and apply knowledge amongst themselves, regardless of the language they speak or the region they come from.

With its based and derivative units, the SI system became an indispensable tool for a whole range of scientific measurements, from measuring chemical reactions in moles to observing cosmic phenomena in kilometers and seconds with measurement sensors.

Healthcare and Medicine

Precision and accuracy are also very important in the medical and healthcare industries and often mean the difference between life and death. Dosages and other fluid measurements are mostly expressed in milliliters, or a thousandth of a liter, which is derived from a unit of volume (cubic meter).

One milliliter equals one cubic centimeter, and it’s a critical measurement in fluid administration, such as administering crystalloid solutions (IV fluids) and intravenous or intramuscular injections. Kilograms, the international unit of weight, is also important in the calculation of medication dosages, usually milligrams or milliliters of medication per kilogram of body weight.

Industry and Commerce

International trade and industrial efficiency also rely on the international system of measurement since it enables seamless interactions and transactions across the globe. The SI units are important in ensuring that products meet strict specifications for weight, dimensions, and production times.

For example, the food industry measures ingredients in grams and milliliters, while the electronics sector operates on volts and amperes (amps), and commerce relies on the SI system to standardize the measurement of goods, shipping volumes, and transportation distances—which are important for logistics and supply chain management.

Summary

The international unit system is more than just a technical framework; it’s a universal language of measurement that spans entire disciplines, cultures, and industries. Its evolution from a revolutionary idea to a universal standard reflects the societal endeavor for precision, understanding, and cooperation.

Are you ready to elevate your measurement and precision standards with non-contact measurement devices?
Contact KEYENCE now to see how our innovative solutions can help streamline your processes and boost your productivity.

Contact us to learn more about how our advanced technology can help take your business to the next level.

Contact Us