• Font Size
  • Normal
  • Large

CHAPTER 4PRESSURE LOSS
FACTORS THAT CAUSE "PRESSURE LOSS"

Pressure loss: The cause of various production line problems

If production line pressure is lost, various problems can occur. This section introduces what pressure loss is, what causes pressure loss, and what countermeasures can be taken to prevent pressure loss.

[1] NARROWING THE PIPE DIAMETER

Restricting the flow path means that piping joints with different diameters will result in pressure loss.

[2] BENDING THE PIPING

Turbulent flow occurs in bent sections, making it difficult for fluids to flow. When this happens, laminar flow changes to turbulent flow and energy loss occurs. Energy loss leads to lowered pressure.

[3] INSTALLING AN OPEN/CLOSE VALVE

If ball valves and other such valves are left fully opened, then pressure loss should not be a concern. However, with valves that change the flow path inside the valve, pressure loss will occur even if fully opened.

Ball valve

When fully opened, it forms a free-flowing structure, so there is no pressure loss.

Globe valve

Even if fully opened, the flow path is changed, resulting in pressure loss.

[4] INSTALLING A FLOW METER

As stated in the operating principles, differential pressure flow meters (diaphragm types) create pressure loss from flow restricting plates to measure flow. Additionally, Karman vortex flow meters restrict and accelerate the flow path in order to provide stable vibrations for the piezo element. Also, with paddle wheel flow meters, the flow path is restricted in order to generate enough thrust to spin the paddles when there is small flow. For these types of flow meters, pressure loss occurs easily. Conversely, with electromagnetic, non-insertion thermal, and ultrasonic flow meters, there is no need to restrict the flow path for detection, which stands as a sizeable advantage in regard to pressure loss.

Back to INDEX

Back to page top

To solve the problem related to the Flow Sensor!