Newer flow meters sometimes include built-in indicators. This is because it is extremely difficult to make accurate settings without a numerical display. Flow within piping can be determined by physical elements such as pipe diameter, the pressure that creates the liquid flow, and the viscosity of the liquid. However, if actually questioned as to how much flow is in the pipe, there is no simple way to know the precise amount. Even if attempting to issue a precise low limit alarm using a flow meter without an indicator, "gauging" must be performed using the procedures below.
MEASURE NORMAL FLOW |
|
---|
PERFORM ALARM SETTINGS |
|
---|
CHAPTER 1
INTRODUCTION TO FLOW METERS
CHAPTER 1
INTRODUCTION TO FLOW METERS