Home  >  What is area roughness?  >  Area Roughness Parameters

Vvc (Core Void Volume) | Area Roughness Parameters


Vvc (Core Void Volume)

Vvc (core void volume) represents the difference between the void volume at areal material ratio p% and the void volume at areal material ratio q%. It can also be used to quantify the magnitude of the core surface, reduced peaks, and reduced valleys based on volume parameters.

Vmp, Vmc, Vvc, and Vvv represent the volumes of the reduced peaks, core material, core void, and valley void respectively.

To use volume parameters, the areal material ratio values that divide the reduced peaks and reduced valleys from the core surface must be specified. By default, 10% and 80% are used.

Vvc (Core void volume)


Find from the parameter list

Height Sa (arithmetical mean height)
Sz (Maximum height)
Sq (Root mean square height)
Ssk (Skewness)
Sku (Kurtosis)
Sp (Maximum peak height)
Sv (Maximum pit height)
Spatial Sal (Auto-correlation length) / Str (Texture aspect ratio)
Std* (Texture direction)
Hybrid Sdq (Root mean square gradient)
Sdr (Developed interfacial area ratio)
Functional Smr(c) Areal material (bearing area) ratio
Smc(mr) Inverse areal material ratio
Sk(Core height)
Spk (Reduced peak height)
Svk (reduced dale height (reduced valley depth))
Smr (Peak material portion)
Smr2 (Valley material portion)
Sxp (Peak extreme height)
Functional volume Vvv (Dale void volume)
Vvc (Core void volume)
Vmp (Peak material volume)
Vmc (Core material volume)
Feature Spd (Density of peaks)
Spc (Arithmetic mean peak curvature)
S10z / S5p / S5v / Sda(c) / Sha(c) / Sdv(c) / Shv(c)



Back to top

Other Pages