A |
Adhesive residue |
Adhesive residue is caused by fracturing of the adhesive (glue) layer. There are three major types of fractures. An anchor fracture is a phenomenon where an adhesive layer is separated from the substrate and transferred to the target. A cohesive fracture is a phenomenon where an adhesive layer is divided and adhered to both the substrate and target. An interfacial fracture is a normal (clean peeling) state. |
Air entrainment |
A defect where air gets trapped in the coating. This occurs when coating is applied too quickly and air gets trapped between the substrate and the coating. |
All-solid-state battery |
Also known as all solid type, these batteries use inorganic solid electrolytes instead of the organic liquid electrolytes and separators used in current lithium-ion batteries (LiB). Solid electrolytes offer greater flame resistance and thermal and chemical stability, which ensures safety and durability even when the energy density is increased. This technology is a promising option for ultra-fast recharging, and structures without liquid electrolyte allow for a higher degree of design flexibility. Research and development efforts toward practical use in electric vehicles (EVs) and other applications are currently underway.
- Related pages
-
|
Anchor effect (Fastener effect) |
An effect where adhesive hardens on the uneven surfaces of a target to form nail or wedge-like shapes. Also called the fastener effect.
- Related pages
-
|
Aspect ratio |
For rectangles, the aspect ratio is the ratio between the lengths of two neighboring sides. For cylindrical objects, the aspect ratio refers to the ratio between the diameter and height. For 3D structures, the aspect ratio is determined from the shape of a cross-sectional view. In linear coating, the state where the thickness is large with respect to the line width is called a high aspect ratio.
- Related pages
-
|
C |
CFRP |
An abbreviation for Carbon Fiber Reinforced Plastic. CFRP refers to composite materials made of carbon fiber and resin. These materials have lower density, less weight, and higher strength than iron or aluminum. Unlike metals, CFRP offers high elasticity and strength in the fiber direction, which enables stronger designs based on the proportion of the fiber direction. CFRP has been used for applications that take advantage of the lightweight, high-strength, and high-rigidity (hard to bend) characteristics, such as in aerospace industry, automotives, and sports gear/equipment.
- Related pages
-
|
Cascading |
A coating defect that looks like ripples on a coated surface. Contrary to "ribbing (longitudinal raised streaks)" caused by the fast speed of the substrate, cascading often occurs when the speed of the substrate is slow.
- Related pages
-
|
Cell pattern transfer |
When a gravure coater is used for thick film coating and the inner volume of the gravure cells—the cells on the roller that create the coating pattern—is increased, the cell pattern becomes coarse and the pattern of the cells themselves is transferred onto the target surface. This coating defect is called cell pattern transfer. |
Chamber |
An enclosed area where coating fluid is applied to a rotating applicator roll using a tank or pump. Chambers prevent the coating fluid from being exposed to air prior to coating. A unit that features a doctor blade at the end of the chamber is called a doctor chamber.
- Related pages
-
|
Changeover |
Changeover refers to the preparation before a process begins where the type of product or the manufacturing method is changed. This preparation includes changing tools, performing reference adjustments of equipment and tools, and changing the materials or components.
- Related pages
-
|
Coating nozzle, coating needle |
The part of a dispenser where the solution is dispensed. A wide variety of coating nozzles/needles are available to suit various coating fluids, purposes, and conditions. In terms of material, for example, metal and plastic needles are used for general purposes, and PTFE nozzles are used for anaerobic solutions. In terms of mechanism, double-threaded screw needles are used for improved stability of the syringe attachment. As for size and shape, precision nozzles and high-resolution nozzles support precision coating, and curved nozzles allow coating on the sides of targets. Various other nozzles and needles are also available. |
Contact angle θ |
References the interior angle between the sidewall of a drop of liquid and the surface it sits on. It can be expressed through Young's equation and represented by θ (Contact Angle). The solid surface is considered wet when the surface tensions of the liquid and solid surface are balanced (the contact angle θ approaches 0).
- Related pages
-
|
D |
Die |
A die is a specially shaped block used to shape an object from a solid material. A mold is used for the same purpose, but instead using molten material. A slot die coater is a coating system that uses a die. Such systems are categorized as pre-metered coating systems that control flow rate through a metering pump before coating. Because these systems ensure a uniform flow rate, width, and speed for coating film forming, they are often used for coating optical films, which require highly accurate film thickness. There are also multi-layer slot die coaters that create multiple layers of coating films simultaneously.
- Related pages
-
|
Dip coating |
A coating method that involves immersing a workpiece (coating target) in solution. After immersion, the workpiece is removed with consideration of the viscous force and surface tension of the solution, gravity, and the removal speed. Any remaining solution on the workpiece is removed through drying or sintering to form a uniform thin film.
- Related pages
-
|
Doctor blade |
A device for removing dirt or foreign particles on the surface of coater rollers that may cause defective coating. Some applications involve intentionally applying more coating fluid than necessary, and a blade removes the excess fluid to control the film thickness to a uniform amount. This blade is also called a doctor blade.
- Related pages
-
|
Drying curve (drying characteristic curve) |
A material property indicated as the amount of moisture evaporation over time per unit of surface area to be dried (or per unit of anhydrous material weight). |
F |
FPC |
An abbreviation for Flexible Printed Circuit, which can also be called flexible PCB, flexible circuit board, flexible printed board, or flexible printed wiring board. An electronic circuit is formed on a substrate consisting of a thin base film which works as an insulator (plastic, polyimide, PET, etc.) and conductive metal such as a copper foil bonded on it. FPCs have been used for smartphones, LCDs, and other electronics because of they are thin and flexible. Major applications include moving parts, bending parts, and cables connecting PCBs, or for units that require thinner and lightweight designs.
- Related pages
-
|
Filler |
Fine inorganic or organic particles that will be added to a resin to improve the functionality. As developments in nano technology continue to arise, fillers of ultrafine particles with micrometer-scale or nanometer-scale diameters have become more popular.
- Related pages
-
|
P |
Photolithography |
A technology where a coat of light-sensitive resist is applied to a substrate before the substrate is exposed to light to form the desired pattern of exposed and unexposed areas. Photolithography is used for nano-order wiring and microfabrication, such as wiring on semiconductor ICs.
- Related pages
-
|
Polymer molecule (Macromolecule) |
A very large molecule. The size of a molecule is expressed by the molecular weight, with larger molecules having a high molecular weight, and smaller molecules having a low molecular weight. In general, a molecule with a molecular weight of several thousands or more is called a polymer molecule or a macromolecule. |
Potting |
In general, potting is a process of filling a case with insulation material such as urethane, silicon, or epoxy in order to protect the electronic circuit mounted inside. Three-dimensional coating using urethane resin for design purposes is also called potting.
- Related pages
-
|
Primary bonding force |
This term is used for adhesive-based adhesion and refers to the force of the chemical bond (such as the covalent bond, metallic bond, or ionic bond).
- Related pages
-
|
S |
Sealant |
Also called sealing material or sealing agent. This paste-like material is made of synthetic resin or synthetic rubber and is used to fill seams or gaps for the purpose of adding water resistance or airtightness. In the sealant coating process, some base coating materials are often used together, such as a sealer—which improves adhesion to the target surface—and primer,—which increases adhesion. Consequently, in the field of automotive manufacturing or construction painting, sealer or primer may be used as a term for sealants.
- Related pages
-
|
Shearing |
An operation similar to cutting an object with scissors. Shearing occurs when two forces parallel to the cross sectional surface of an object are applied in opposite directions.
- Related pages
-
|
Slurry |
A muddy or gruel-like mixture of solid particles suspended in liquid. Also called a slip.
- Related pages
-
|
Solidification |
A process where a liquid or gas turns into a solid. Solidification is synonymous with “coagulation”. The process is generally differentiated for gases under the term “sublimation”.
- Related pages
-
|
Streak |
A defect that appears on a coated surface (also known as linear defects). Many causes may contribute to this type of defect. For example, when a large particle is caught on part of the coating equipment, such as a blade for adjusting the coating amount, a linear defect will be created on the coated surface.
- Related pages
-
|
Substrate |
A base material used for making products or compounds. A smooth film or sheet substrate wound into a roll is called a web.
- Related pages
-
|
Surface tension |
Surface tension is the force operating on a liquid to continually minimize its surface area. It is caused by the attraction among the molecules to pull surface molecules inward.
- Related pages
-
|
Syringe |
For industrial use, a syringe refers to a type of pump that continuously feeds liquid such as adhesive, silver, solder paste, grease, or solution from a container.
- Related pages
-
|