TEL
  1. Home
  2. Solutions
  3. Case Studies
  4. KEYENCE VHX-7000 4K Digital Microscope helps archaeologists improve their understanding of the ancient world

KEYENCE VHX-7000 4K Digital Microscope helps archaeologists improve their understanding of the ancient world

The Archaeology Department of the University of Liverpool has carried out two ground-breaking projects that have improved our understanding of how human culture developed in ancient times. Playing a key role in that research has been the KEYENCE VHX-7000 Series Digital Microscope, the world's first 4K ultra-high accuracy microscope.

Elizabeth Thomas, an Archaeology PhD student at the university, had the opportunity to use the KEYENCE digital microscope when conducting research for her Masters and PhD. This work involved analysing Egyptian mirrors, many of them dating back to the Middle Kingdom era of the 12th Dynasty.

The VHX-7000 was used to gather information on the different kinds of corrosion found on the mirrors. Elizabeth felt it was important to see the different layers in the mirrors and how they were made, which was not possible using a scanning electron microscope (SEM) where image delivery was in grayscale.

Essential for Elizabeth’s work was the ability to create colour images and show extremely high levels of detail at high magnification settings. Having access to full-colour high magnification images was vital to ascertain how an artifact might have looked in its original state.

Elizabeth found that another benefit of using the KEYENCE digital microscope was that it could display textiles that had been preserved in corrosion. The VHX-7000 was able to capture images of these textiles for subsequent examination by an expert.

In addition, the digital microscope made stitching images a straightforward process, whereas an SEM would require image stitching to be carried out manually using separate software. The VHX-7000 also eliminated the need for preparing samples – an SEM requiring them to be secured on to a stand – while the measurement capabilities of the KEYENCE system saved Elizabeth a considerable amount of time.

“There are many advantages to using the VHX-7000,” says Elizabeth, “and it represents a massive jump in functionality from any previous digital microscopes I’ve used. For example, the flexibility of being able to move the unit’s fully-integrated head around a sample is invaluable. It means that just by tilting the head, it’s possible to create multiple views of the same sample.”

In a second project involving the University of Liverpool’s Archaeology Department, the VHX-7000 was used to carry out laboratory-based archaeobotanical analysis of delicate and highly valuable charred plant macrofossils. Some 966 non-wood items and 440 wood charcoals were retrieved from excavations at the Palegawra cave, a Zarzian occupation site in north-eastern Iraq.

This culture dates from the late Palaeolithic and Mesolithic eras and it has been possible to discover a great deal of new information about it by studying well-preserved botanical and faunal remains. This research was carried out by the Eastern Fertile Crescent (EFEC) project, a collaboration between the University of Liverpool and the Sulaymaniyah Directorate of Antiquities and Heritage.

What makes the EFEC project stand out from any similar projects is that the team at the university understood early on that the traditional method of using a scanning electron microscope had significant limitations, as Elizabeth had found out in her work. The team realised that relying on this type of equipment could reduce the effectiveness of sample analysis and the quality of data.

Another key reason the team preferred the KEYENCE microscope was that the wood charcoal specimens would be better protected, and the non-wood charred macrofossils could be retained as completely as possible for future analysis. Wherever possible, all analysis was carried out on a non-destructive basis and the KEYENCE VHX-7000 helped to achieve this.

Many wood charcoal specimens collected from the caves were photographed using the VHX-7000 at magnifications of between 100x and 1000x. Thanks to the quality of images obtained, botanical identifications were made by comparing the samples with published works and specimens held in Liverpool’s own wood charcoal reference collection.

Archaeologists have found that the VHX-7000 can help to identify subtle contours and uneven surfaces or stains that would otherwise be impossible to see, thanks to Optical Shadow Effect Mode delivering high-definition capture.

Ease of use is another key feature, with the KEYENCE microscope offering a fully automated system. By simply turning a dial, magnification can be moved from 20x to 6000x and there is no need to replace any lenses.

KEYENCE is delighted that the VHX-7000 Series Digital Microscope was able to play such a major role in these projects, and in improving archaeologists’ – and humanity’s – understanding of our ancient world.

APPLICABLE PRODUCT CATALOG

Related Products

  • VK-X3000 series - 3D Surface Profiler

    The VK-X3000 3D Surface Profiler uses a triple scan approach, where laser confocal scanning, focus variation, and white light interferometry measurement methods are used, so that high-accuracy measurement and analysis can be performed on any target. The VK-X3000 has a resolution of 0.01 nm and can scan areas up to 50 × 50 mm (1.97″ × 1.97″), allowing for measurement of the overall shape of the target while still maintaining high-resolution for analysis of minute surface features. KEYENCE's new 3D Surface Profiler can handle any target, including those with transparent or mirrored surfaces, large height changes, or steep angles.

  • VR-6000 series - 3D Optical Profilometer

    The VR-6000 optical profilometer performs non-contact measurement to replace stylus profilometers and roughness meters. This 3D profile system captures full surface data across the target with a resolution of 0.1 µm, enabling measurement of features that cannot be performed with probe-type instruments. The new rotational scanning greatly expands the measurement capabilities of the system. True-to-life cross section measurements can be performed with no blind spots. Wall thicknesses and recessed features can be measured without cutting or destroying the target. In addition, the HDR scanning algorithm provides enhanced scanning capabilities for instantly determining the optimal settings to capture high quality data, even on glossy and matte surfaces.

  • VL-800 series - 3D Scanner CMM

    The VL-800 Series 3D Scanner CMM is the first in its lineup to feature 3D-AI, making high-quality 3D data acquisition and analysis effortless for any user. The system intelligently recommends optimal scanning, stitching, and measurement methods based on the shape of the part being analyzed. Additionally, scanned parts can be directly compared to their CAD models for quick visualization of differences, or the 3D scan can be used to streamline reverse engineering processes. From scanning to STEP file output, the VL-800 handles everything automatically, and provides accurate data in a format accessible by any CAD software.