Pokayoke (Error-Proofing)

Mechanisms for detecting or preventing the generation of defects caused by careless mistakes, which are unavoidable at manufacturing worksites, is referred to as pokayoke (error-proofing). This section introduces items such as basic knowledge pertaining to careless mistakes and pokayoke (error-proofing), the way to use a handheld computer system to perform pokayoke (error-proofing) and the advantages of doing so, how to install handheld computers, and the flow for operation of handheld computers.

What Is Pokayoke (Error-Proofing)?

User-caused errors occur at manufacturing worksites and lead to defects.

These user-caused operation errors are generally referred to as careless mistakes. The mechanisms for preventing the occurrence of careless mistakes and for preventing defective products from mixing in with good ones even if careless mistakes occur are referred to as pokayoke (error-proofing).

These mechanisms are separated into defect prevention (error stoppage, mistake restrictions, and prevention alarms) and defect detection (defect stoppage, flow restrictions, and occurrence alarms). It is also possible to identify the causes of defects and the processes in which they occurred, which makes it possible to develop improvement strategies for preventing the reoccurrence of defects.

In summary, pokayoke (error-proofing) refers to the mechanisms for notifying users of the occurrence of defects, preventing defective products from mixing with good ones in the rare event that defects occur, and preventing the reoccurrence of defects.

Pokayoke (Error-Proofing) With Handheld Computers

There are various causes of careless mistakes at manufacturing worksites. Just a few examples are incorrectly reading product numbers, taking the wrong part, making mistakes in the setting of molds and jigs, and making mistakes in the blending of raw materials. Careless mistakes such as these can be prevented by thoroughly performing verification with handheld computers. This section introduces pokayoke (error-proofing) using handheld computers.

Pokayoke (Error-Proofing) With Shipping Inspection and Actual / Sign Product Verification

The possibilities of incorrect parts being shipped and part shortages occurring during shipping can be reduced to nearly zero by performing a duplicate check in which the barcodes and 2D codes on the customer sign and the in-house sign are read. The pokayoke (error-proofing) effect can be further increased by performing three-point verification visually by displaying the target image on the LCD of the handheld computer.

Shelfing Pokayoke (Error-Proofing) When Stocking / Restocking Parts

To prevent accidental introduction of items onto shelves when stocking / restocking parts and raw materials, affix item labels (barcodes) to parts and product number barcodes to the part shelves, and then use handheld computers to verify both barcodes. With visual inspection, it is possible that similar parts will be introduced accidentally, but management with barcodes can prevent careless mistakes when shelfing parts.

Recipe Checks When Blending / Compounding Raw Materials

When beginning production or during tool changeovers, blending and compounding mistakes can be prevented by verifying the manufacturing instructions against the barcode of the raw materials to be inserted.

  • A
    Manufacturing instructions for input materials
  • B
    Input materials

Checking the Setting of Molds and Jigs

During production of small lots of a wide variety of products, tool changeovers occur frequently and similar molds and jigs may be used. This may lead to mistakes in the setting of molds and jigs. Such mistakes can be prevented by affixing barcodes to molds and jigs in advance and verifying the manufacturing instructions against the molds and jigs.

  • A
    Core
  • B
    Cavity
  • C
    Manufacturing instructions

Advantages Provided by Handheld Computers

This section introduces the advantages of installing handheld computers for pokayoke (error-proofing).

Eliminating Careless Mistakes Caused by Taking the Wrong Product Among Similar Ones

As the number of products whose outer appearances are similar increases, these products may look the same to inexperienced operators. Careless mistakes caused by taking the wrong product can be eliminated by affixing barcodes or 2D codes to products and having operators read these codes with handheld computers during confirmation.

Able to Output Data and Signals to the Control Device

By outputting the data read by the handheld computer to an indicator, interlock, or other such control device, notification of an error occurring when verification fails can be provided with the indicator and the interlock can be released when verification passes. This makes it possible to eliminate careless mistakes in various operations.

Sending Work Data to a PC or Server in Real Time

Data read with a handheld computer can be sent to a PC or server in real time. This makes it possible to monitor the occurrences of careless mistakes from the headquarters or an office. Notifications of careless mistakes are given in real time and the work information from preprocessing can also be checked, so this is effective in identifying the causes of careless mistakes.

Related Downloads

Handheld Mobile Computer: Error-Proofing, Simple Confirmation and Elimination of Mistakes

How to implement Handheld Mobile Computers to error-proof processes and inspections.

Download

Handheld Mobile Computer Application Guide BASIC CONCEPTS AND INSTALLATION EXAMPLES

This guide summarizes the applications of handheld mobile computers. It provides easy-to-understand descriptions, from basic knowledge such as the abilities of handheld mobile computers, the environment required for installation, and successful applications, to installation examples by industry and important points on selecting handheld mobile computers.

Download

Handheld Mobile Computer: Logistics Operations, Eliminating Shipment Errors

This document summarizes solutions to eliminate shipping mistakes in the logistics industry. It describes ways to use handheld mobile computers to prevent mistakes when packages have no barcodes and to solve problems in various processes such as receiving, shelving, picking, and shipping inspection.

Download

Barcode Solutions for Logistics

This document covers the system of logistics and basic knowledge of operations, the roles required of next-generation logistics, methods to improve efficiency, and operation improvement examples. It is packed with useful information and recommended to everyone involved in logistics from beginners to experts.

Download