Changes in Two-dimensional Code Verification

The history of two-dimensional code verification began in 2000, and the standards have been revised over time.

The following illustration shows how code verification standards have changed from 2000 to today.
As the marking target has shifted from labels (paper) to objects such as metal and resin, new standards have been created.

Label

In addition to definitions related to the composition of codes, this standard also contains definitions related to marking quality. The version of this standard from the 2000 fiscal year is the main standard.

・ISO/IEC 16022DataMatrix symbol standard ・ISO/IEC 18004QR code symbol standard ・ISO/IEC 15415:2004The first version of the standard for marking quality verification ・ISO/IEC 15415:2011The second version of the standard for marking quality verification + Additional information DPM ・AIM DPM-1-2006A DPM two-dimensional codemarking quality verification standard established by Automatic Identification Manufacturers (AIM) and that is based on ISO/IEC 15415:2004 ・ISO/IEC TR 29158A DPM two-dimensional code marking quality verification standard established by the International Organization for and that takes into account both ISO/IEC 15415:2011 and AIM DPM-1-2006

INDEX