Laser Marking Systems / Laser Markers
Why Valve Marking is Essential for AI Server Cooling
-
Tags:
- Laser Marking , Laser Etching , Semiconductor
As most are now aware, the AI market is rapidly expanding. From ChatGPT, Gemini, and enterprise use cases, every AI-powered application requires proper servers to make the magic happen. In 2024, the market value of AI servers is expected to reach $187 billion, representing 65% of the total server market. Future growth expectations are also staggering, as AI servers are projected to continue growing at a rate of 41.5% year-over-year.
What is behind this upward trajectory? Most industries are now utilizing AI technologies, such as finance, healthcare, and technology. However, outdated server infrastructure won't cut it any longer, as efficient cooling systems are needed to handle the heat generated by these advanced AI applications. Without them and components like valves, overheating occurs, affecting operations.
Valves help manage the flow of fluids (in this case, cooling fluids), which then maintain the necessary temperature levels. Given the significant heat produced by AI servers due to their intensive processing power, cooling systems must operate efficiently to prevent disastrous performance issues. In short, precise temperature control is possible because of valves, helping the system maintain optimal conditions.
Data centers produce a ton of heat and rely on complex AI server cooling systems. If the valves being used are not correctly marked, technicians can not quickly identify and manage these components, reducing the risk of system downtime. Server maintenance is also a necessity, and marked components are helpful. Without traceability, technicians may also experience delays in adjusting or replacing critical parts, which could lead to cooling inefficiencies or even worst-case scenarios like system failures.
In environments where AI workloads are operated 24/7, laser marking valves ensure that the cooling process remains precise and uninterrupted. Clear, accurate identification of valves and other cooling components allows airflow to be controlled more effectively, and repairs or replacements can happen swiftly.
In high-pressure AI environments, the accuracy and clarity provided by valve marking systems reduce errors and improve safety and operational efficiency. Keeping servers at peak performance is at the top of the priority list, as business revenues and overall functionality rely on it.
Valve Marking Standards for AI Data Centers
Standards, regardless of the industry or use case, serve as essential guidelines to ensure consistency, reliability, and safety. When in place, a unified framework is available for operations and technicians. Seamless collaboration, quality assurance, and compliance are then possible. Data centers and all cooling components need to follow the same standards. Valves and pipes, for example, require clear labels to make maintenance easier and help prevent mistakes.
Since AI servers produce high amounts of heat and run continuously, valve markings need to be resistant to wear, temperature fluctuations, and moisture. Proactively implementing marking standards allows facilities to meet these challenges and requirements. Operational consistency improves, errors are minimized, and all components are clearly identified across different sites.
We’re here to provide you with more details.
Reach out today!

Types of Valve Marking Tags for AI Server Cooling Systems
A valve marking tag is an identification tool used in various industries, including data centers, to label and indicate the function, type, and operational status of valves within a system. Service technicians can then use the tags to identify valves for maintenance, adjustments, or replacements. Durable and legible tags are non-negotiable, especially in environments like AI data centers.
There are several types of valve marking tags used in AI server cooling systems, each serving a specific purpose:
- Laser-etched tags: Highly durable and precise, laser-etched valve tags can withstand extreme conditions and remain readable over time. Tags that are laser-etched offer a lasting, durable solution for identifying components in AI data centers that operate at high temperatures.
- Color-coded labels: These provide a quick and easy way to differentiate between various valves, helping technicians quickly locate the right part during routine maintenance or emergency repairs.
- QR code tags: By scanning QR codes, technicians can access real-time data about a valve’s function, history, and maintenance schedule, enabling faster decision-making.
Regardless of the type of valve marking tag used, there are some benchmark practices to keep in mind.
Discover more about this product.
Click here to book your demo.

Valve Marking in Data Center Cooling Systems: Best Practices
There are right and wrong ways to do everything, including valve marking for data center cooling systems. One of the most important factors is choosing high-quality materials for valve tags. If they can’t withstand the elements, it becomes challenging for operators to read and use them effectively over time. The suitable materials will prevent mistakes during maintenance, which can be costly and lead to delays in cooling operations.
Consistency also helps in terms of data center operations. For example, a standardized marking system makes it easier for technicians to locate and service valves quickly. Every second of the day, AI data centers are collecting and processing massive amounts of data. Overheating and equipment failure can be avoided or minimized when valves and components are properly marked.
Automating the laser valve marking process can take efficiency to the next level. Automation makes marking multiple valves more accurate and faster. On the other hand, manual marking methods often experience downtime. By embracing an automated marking system, data centers can maintain a high level of operational efficiency.
Using the right laser marker and following these valve marking standards helps data centers protect the integrity of their AI data centers. But what laser marking systems are best for marking valves? Here are a few options that can assist with different materials:
- 3-Axis Fiber Laser Marker MD-F Series: Known for its high power and efficiency, this fiber laser marker is excellent at marking with depth into the valve surfaces. Deep, permanent markings are created that resist wear and environmental conditions.
- 3-Axis UV Laser Marker MD-U Series: Ideal for marking delicate or sensitive materials without causing damage. The MD-U creates high-contrast, precise markings on plastic valves, valves with environmentally resistant coatings, or labels.
- 3-Axis Hybrid Laser Marker MD-X Series: The MD-X combines the advantages of fiber and YVO4 technologies, with flexibility for marking both metal and non-metal valve components. Perfect for data centers with different materials, it provides clear valve markings regardless of the material.
- 3-Axis CO2 Laser Marker ML-Z Series: For valves with non-metallic surfaces like plastic or coated materials, the CO2 laser provides crisp, non-contrast markings. Efficient for fast marking, it is ideal for large-scale data centers where speed and throughput are critical but where contrast is not necessary.
KEYENCE has the solution for whichever type of valves you require marking on. Following these best practices and choosing the right equipment will save time and costs.
Get detailed information on our products by downloading our catalog.
View Catalog

Optimizing AI Server Cooling with Proper Valve Marking
AI applications are expanding rapidly, and with them, a need for more extensive, efficient data centers. Proper valve marking plays a vital role in optimizing AI servers, as does using the right laser marking equipment. Following the best practices and using industry-leading laser marking systems will improve operational efficiency and safety in AI data center cooling.
Ready to simplify your AI server operations and valve marking processes? Contact us today—KEYENCE has trained specialists and product demos to assist.
We’re here to provide you with more details.
Reach out today!

Related Downloads

KEYENCE's MD-F Series offers unmatched functionality in a compact design.