Laser Marking Systems / Laser Markers
Precision Laser Medical Tubing
-
Tags:
- Laser Cutting , Laser Drilling , Medical
The evolution of laser medical tubing technologies has brought forth some significant advancements in the healthcare industry. Laser medical tubing refers to medical-grade tubing manufactured or processed using laser technology. Lasers offer the unmatched dependability, adaptability, and consistency required for manufacturing medical parts.
Read on to learn how manufacturers are using lasers for medical tubing, how they benefit, and what equipment works best for these applications.
Overview of Laser Medical Tubing Applications
Laser-cut medical tubing is necessary for producing high-precision components for healthcare. It’s used to create stents with intricate designs, ensuring flexibility and durability for minimally invasive procedures. The accuracy of laser cutting enables complex geometries, such as expandable mesh patterns, that allow stents to be compactly inserted into narrow arteries and then expanded securely. This ensures the stent can flex without breaking and maintain structural integrity over time.
Similarly, hypo tubing benefits from laser systems that are capable of achieving sharp, burr-free edges. Medical laser tubing is integral to catheter production, where smooth edges and precise dimensions are essential for patient safety and effective performance. Additionally, laser-cut medical hypo tubing supports drug delivery systems by creating micro-features that regulate drug release.
We’re here to provide you with more details.
Reach out today!

Benefits of Laser Cutting for Medical Tubing
The advantages of laser cutting extend beyond accuracy. Its non-contact nature is particularly vital, ensuring that hypo tubing retains its thin-walled integrity while stainless steel tubing remains robust for medical use demands. This Laser cutting technique helps prevent warping, cracking, or other distortions during processing, which is crucial for flexible components and diagnostic tools.
Other benefits gained by using this technology include:
- Works with intricate geometries: Laser-cutting technology allows for the production of intricate microfeatures and shapes needed for sophisticated surgical and diagnostic tools. For instance, laser-cut patterns in stents enhance their ability to expand and flex during minimally invasive procedures, providing both reliability and precision in performance.
- Provides needed sterility: Laser cutting eliminates the need for secondary cleaning processes by producing burr-free components with sterile, non-toxic finishes. Many medical devices come into direct contact with the body, so ensuring patient safety and regulatory compliance is a priority.
- Offers versatility on different materials: Laser cutting is an all-encompassing solution because it can work with various materials, including polymer-based medical laser tubing, hypo tubing, and stainless steel. As a result, manufacturers can produce many devices suited for diverse medical applications, ranging from flexible catheters to rigid surgical instruments.
Discover more about this product.
Click here to book your demo.

Versatility in Material Handling: Hypo and Stainless Steel Tubing
Laser marking in the medical industry can be challenging. Fortunately, laser cutting can handle diverse materials with precision. For example, hypo tubing, which is often used in vascular surgeries, requires sharp edges and intricate cuts that laser systems deliver effortlessly. Medical tubing made of stainless steel gains from the process's capacity to increase corrosion resistance and durability. Characteristics like these are particularly useful in drug delivery systems, implants, and surgical instruments.
Enhanced Precision with KEYENCE Laser Medical Tubing
KEYENCE’s laser systems redefine standards in the production of medical tubing. Optical zoom technology and intuitive software features simplify the production of complex components. For instance, laser systems ensure the efficient manufacturing of medical laser tubing by automatically adjusting to different materials and production needs. Manufacturers can also optimize workflows and maintain consistency through real-time data analysis.
Laser cutting is popular as it guarantees the highest standards in the manufacturing of medical devices, from complex stents to hypo tubing. Manufacturers can increase efficiency and precision while improving product quality by incorporating KEYENCE's laser marking systems.
Contact us today to learn more about transforming your operations with industry-leading laser systems.
Contact us to learn more about how our advanced technology can help take your business to the next level.
Contact Us