Safety Light Curtain Selection Website: GL-R Series

In situations such as these…

Simply follow the steps below and a dedicated representative will send you a proposal by email.

Feel free to contact us by phone or email if you have any questions regarding your proposal.

Only supported within the United States

List of required light curtain components. / Easier than using the phone!

Select desired features below!

Please enter in single-byte number.
Please enter a number greater than 0.

STEP1 Select the type of main unit.
Select the GL-R Series and move to the next step

Standard type
GL-R Series

  • Robust with no need for additional protection
  • High power for demanding environments
  • Maximum operating distance: 15m
Select the GL-S Series and move to the next step

Slim & flat
GL-S Series

  • Compact for tight spaces
  • Pre-installed mounting brackets
  • Maximum operating distance: 2m

check

The GL-R Series meets most of the needs of our customers.
Select the GL-S Series if you require a more compact type.

Application

STEP2 Select the application.

check

We recommend the 14mm type when distance to the hazard is short.
Reducing the mounting distance can help keep equipment compact.

Next

Series connection

STEP3 Select whether the light curtains will be used with a series connection.

View a series connection usage example

  • Select this if you are unsure!

check

Unless you intend to connect multiple light curtains together, select "Light curtains will not be used with a series connection."

Next

Height

STEP4 Enter the height to protect.

* Use numeric characters to enter the value.

Set 1
inch

Set 2
inch

Set 3
inch

Next

Mounting bracket

STEP5 Select the mounting brackets.
  • Rear mounting → 45° mounting → Side mounting
  • We recommend this bracket when the mounting brackets cannot be installed vertically and when installing the brackets in an L shape.

  • This is a simple mounting bracket. It cannot rotate.

  • This is a simple mounting bracket. It cannot rotate.

Next

Wiring

STEP6 Select the wiring.
  • Detail
  • Detail

check

The optional safety relay provides full light curtain functionality with simple quick disconnect cables.

Next

Length

STEP7 Select the cable length.

Length of (1)

Length of (1)

Length of (2)

Length of (1)

Length of (2)

Length of (1)

Length of (2)

Length of (1)

Length of (2)

Length of (3)

Length of (1)

Length of (2)

Length of (3)

Next

NPN/PNP

STEP8 Select NPN or PNP.

Next

Safety functions

STEP9 Select the safety functions that you plan to use.
* Multiple selections allowed

check

When connecting the output of the light curtain to the safety relay directly, use the EDM function.

Next

Options

STEP10 Select the optional components. * Multiple selections allowed

check

The laser alignment tool is most beneficial for long range applications or applications that require mirrors.

Use the space below for any other requests and questions.

Sign In

If you do not have an account, please create one now. You will only need to do this once.

KEYENCE Site Registration

Create an account now for unlimited instant access to all KEYENCE site resources in the future.

  • * required