Measurement Sensors
- 2D/3D Laser Profiler LJ-X8000 series
- High-speed 2D Laser Profiler LJ-V7000 series
- 2D Laser Displacement Sensor LJ-G5000 series
- Confocal Displacement Sensor CL-3000 series
- Ultra High-Speed/High-Accuracy Laser Displacement Sensor LK-G5000 series
- High-Speed, High-Accuracy CCD Laser Displacement Sensor LK-G3000 series
- Image-Based Laser Sensor IX series
- CMOS Multi-Function Analog Laser Sensor IL series
- Telecentric Measurement System TM-X5000 series
- High-speed optical micrometer LS-9000 series
- High-speed 2D Optical Micrometer TM-3000 series
- High-speed, High-accuracy Digital Micrometer LS-7000 series
- Multi-Purpose CCD Laser Micrometer IG series
- Thrubeam Type Laser Detection Sensor IB series
- 3D Interference Measurement Sensor WI-5000 series
- Micro-head Spectral-interference Laser Displacement Meter SI-F series
- Spectral-Interference Wafer Thickness Meter SI-F80R series
- High-speed, High-Accuracy Digital Displacement Inductive Sensor EX-V series
- Inductive Gauging Sensor AS series
- High-accuracy Positioning Sensor EG series
- High-Accuracy Digital Contact Sensor GT2 series
- General Purpose Digital Contact Sensor GT series
Dimension Measurement
Displacement Measurement
- Measurement Sensors for the Medical and Pharmaceutical Industry
- Measurement Sensors for the Fiber Optic/Cable Industry
- Measurement Sensors for the Film and Sheet Industry
- Measurement Sensors for the Electric Vehicle Industry
- Measurement Sensors for the Semiconductor Industry
- Measurement Sensors for the Electronics Systems Industry
- Measurement Sensors for the Food and Beverage Industry
- Measurement Sensors for the Automotive Manufacturing Industry
- Measurement Sensors for the Metal and Steel Industry
Measuring Angles
When looking for the best way to measure angle, there are several important factors to consider, including the type of measurement system and the installation environment. Selecting equipment that doesn't adequately meet your needs can lead to insufficient precision and increased man-hours during production. This site is designed to help users determine the best way to perform measurements with confidence regarding an angle measurement system.
Angle Measurement with a Reflective-Type Sensor
Angle measurement of bevel during welding
A reflective-type sensor’s primary function is to measure the position of a target based on the light reflected from the target surface. While it is not directly used for measuring angles, it can be used in systems where angle measurements are calculated from the variation in the position of the target.
Optimal Measurement System 2D Triangulation Laser Displacement Sensor
The cross-sectional shape of locations where the laser hits are obtained and the angle is measured based on the shape.
- Angle can be measured using only one head
- Angle can be computed internally
-
1Angle
-
2Cross position (X, Z coordinates)
2D/3D Laser Profiler LJ-X8000 Series
LJ-X laser profilers collect height data across a laser line rather than a single point. This enables 2D/3D measurements such as height difference, width, or angle to be performed using a single sensor.
Click here for more details
- 2D triangulation method
- In-line multi-point measurement
- World's fastest sampling rate at 64,000 images/sec
Confocal Displacement Sensor CL-3000 Series
High-precision measurement on all targets, with simple sensor head installation and program settings. CL-3000 Series ultra-compact coaxial laser displacement sensors address manufacturing challenges such as improving quality, preventing the shipment of defective parts and increasing production.
Click here for more details
- Multi-color confocal method
- Linearity:From ±0.2 µm
- Confocal displacement sensor
Angle Measurement with a Thrubeam-Type Sensor
Angle Measurement of drill tips
Thrubeam sensors, also known as through-beam sensors, are photoelectric sensors that consist of a light emitter, which emits the light, and a light receiver, which monitors the presence of that light beam. These components are positioned facing each other, and the detection occurs when the light beam between said components is interrupted by an object.
Thrubeam sensors are well-known for their high levels of accuracy, as they’re not affected by the color of the object, its texture, or the object's reflectivity, making them perfect for measuring angles in numerous industries and applications.
Optimal Measurement System Thrubeam 2D Optical Micrometer
The angle at specified points is measured using the image obtained using the 2D optical projection method. In addition to angle; the outer diameter, step, and other parameters can also be measured for multiple locations at the same time.
-
1Angle
-
2Inclination from virtual line
Telecentric Measurement System TM-X5000 Series
TM-X optical micrometers are thrubeam sensors that measure any object that blocks the light passing from the transmitter to the receiver. These sensors are designed without moving parts to provide accurate measurements without regular maintenance.
Click here for more details
2D telecentric optical method. Simultaneous measurement of up to 100 with calibrated high-speed measurement.
What is Angle Measurement?
Measuring angles is a process of determining the position or orientation of an observed object relative to a reference angle. These measurements are typically performed using manual methods. However, in certain situations, physical measurements are unreliable due to human error and the angle measurement tool’s resolution or due to the fragile nature of the object, in which case physical measurements might end up damaging the object.
That’s where non-contact measurement methods come in—more specifically, laser scanners and optical measurement systems. Admittedly, these two angle measurement systems rely on different working principles, but they’re incredibly accurate, and their accuracy typically ranges within the micron level.
What is Needed to Measure Angles
Each of the aforementioned angle measurement methods and their respective product lines can be used to measure angles and positions relative to a reference angle. The 2D triangulation sensors determine the position of a point in two dimensions and use the recorded positions to derive the angle.
Multi-color confocal sensors use chromatic aberration to determine the distance between the sensor and the surface and indirectly measure angles. Thru-beam sensors can be used for measuring angles, or they can be a part of a measuring system that can derive the angle based on the interpretation of the beam.
As such, it’s important to note that 2D triangulation and multi-color confocal sensors directly measure angles by determining the position of a point on a surface of the part, while thru-beam sensors can be used to derive the angle based on the 2D optical projection principle.
What are Easy Ways to Measure Angles?
When it comes to measuring angles in a professional and industrial setting, “easy” can be different from what’s required, especially with precision manufacturing of complex shapes. These settings typically require the use of more sophisticated angle-measuring methods and equipment, like those mentioned above.
In this case, the ease of measuring angles comes from the equipment’s capability to automate the angle-measuring process and provide accurate results. This effectively excludes the need for extensive manual interventions, measurements, and calculations. So, the easiest way to measure angles is to rely on properly calibrated angle-measuring automation solutions.
Related Downloads
This guide contains a wide range of measurement methods: thickness, width, height/step, outer diameter, stroke, run-out/vibration, eccentricity, warpage/flatness, angle, gap/clearance, target meandering, radius, inner diameter, positioning, profile, and 3D shape.
Related Products
Applications
Dimension Measurement
Displacement Measurement
Profile Measurement
Industries
- Measurement Sensors for the Medical and Pharmaceutical Industry
- Measurement Sensors for the Fiber Optic/Cable Industry
- Measurement Sensors for the Film and Sheet Industry
- Measurement Sensors for the Electric Vehicle Industry
- Measurement Sensors for the Semiconductor Industry
- Measurement Sensors for the Electronics Systems Industry
- Measurement Sensors for the Food and Beverage Industry
- Measurement Sensors for the Automotive Manufacturing Industry
- Measurement Sensors for the Metal and Steel Industry