TEL

VJ Series User Support Site

VJ SeriesSoftware

This page introduces how to download the latest software and how to activate the software (Function Activation).

Software Downloads Activation (Function Activation)

Software

This software is used to connect the VJ Series to a PC over GigE and to configure the settings. This download contains:
-VJ Editor + VJ Utility + VJ Simulator*
-VJ Libraries for C/C++/C#(.NET)
* When using the simulator function, click here for activation.
This file is used to update the firmware on the VJ series image processing unit.

Drivers for Each Image Processing Library (in alphabetical order)

This driver is required when using the VJ Series with HALCON.
This driver is required when using the VJ Series with LabVIEW.
This driver is required when using the VJ Series with NeuroCheck.
This library is used to connect the VJ Series and a PC over GigE. This download contains VJ software and the library. To acquire the library only, just select "Image acquisition runtime library for VJ Series" when running the installer.
  • *No driver is required when using VisionPro or MatroxImagingLibrary (MIL).
  • *Click here for connection manuals and sample code for each image processing library.
  • *Product names are trademarks or registered trademarks of their respective companies.