VS Series E-Learning
Tool Tutorial exercises that explain the key settings of the main inspection tools.
Using the Simulator
Importing a Setting File
How to import a setting file into the VS creator software.
Tools
Area
Presence/Absence inspection by counting the number of white or black pixels on a binary image.
Blob
Count, sort, locate and analyze clusters of white or black pixels extracted from a binary image.
Defect
Detects & analyzes areas with a specified intensity difference by comparing the average intensity in smaller segments to the neighboring segments.
Grayscale Blob
Counts & analyzes clusters of lighter or darker pixels that are detected based on a specified intensity difference compared to the average background intensity.
Pattern Search
Detects & locates a specified grayscale pattern which can also be used for position adjustment for other tools.
ShapeTrax3A
Detects & locates a specified pattern based on edge feature information around the profile of the target which can also be used for position adjustment for other tools.
Edge Position
Locates the position of an edge and/or counts the number of edges present.
Edge Pitch / Edge Pairs
Detects pairs of edges and measures the min., max., and ave. distance between the pairs. It can measure center pitch or gap pitch.
Edge Width / Profile Width
Detects multiple edges and measures the distance between two specified edges. Also detects the min. & max. width along a profile.
Profile Position / Profile Defect
Detects multiple edge points along a profile. The min. & max. position can be detected as well as best fit shape. Defects that deviate from the best fit shape can also be detected.