Sensor Network Device Software
Applicable models: NQ Series / IO-Link-compatible sensors
NQ Sensor Monitor
Monitoring software
NQ Sensor Monitor
This is setup/monitoring software for the NQ Series.
EtherNet/IP® Configuration Files
EtherNet/IP® configuration files (AOI files)
NQ Series Add-On Instruction for Allen-Bradley PLC
NQ Series [EtherNet/IP™] Connection Guide [Allen-Bradley CompactLogix Edition]
This is an easy connection guide that covers topics from connection methods to settings, enabling users to communicate with devices.
Communication Configuration Files
EtherNet/IP® configuration files (EDS files)
[NQ-MP8L] Setting file for EtherNet/IP™ (EDS file)
This is an NQ-MP8L EtherNet/IP™ communication configuration file (EDS file).
[NQ-EP4L] Setting file for EtherNet/IP™ (EDS file)
This is an NQ-EP4L EtherNet/IP™ communication configuration file (EDS file).
[NQ-EP4A] Setting file for EtherNet/IP™ (EDS file)
This is an NQ-EP4A EtherNet/IP™ communication configuration file (EDS file).
PROFINET communication module configuration file (GSDML file)
[NQ-MP8L] Communication module setting file (GSDML file)
This is an NQ-MP8L PROFINET communication configuration file (GSDML file).
EtherCAT communication module configuration file (ESI file)
[NQ-EC8L] Communication module setting file (ESI file)
This is an NQ-EC8L EtherCAT communication configuration file (ESI file).
KV STUDIO communication unit configuration files (ez1 files)
[NQ-MP8L] Communication Unit Configuration File for KV STUDIO(ez1 file)
This is an NQ-MP8L KV STUDIO configuration file (ez1 file).
[NQ-EP4L] Communication Unit Configuration File for KV STUDIO(ez1 file)
This is an NQ-EP4L KV STUDIO configuration file (ez1 file).
[NQ-EP4A] Communication Unit Configuration File for KV STUDIO(ez1 file)
This is an NQ-EP4A KV STUDIO configuration file (ez1 file).
IO-Link Configuration Files
IO-Link configuration files (IODD files)
[NQ-IL8P] IO-Link Configuration File (IODD File)
This is the setting file to use when connecting the NQ-IL8P to an IO-Link master.
[LR-X Series] IO-Link Configuration File (IODD File)
This is the setting file to use when connecting the LR-X Series to an IO-Link master.
LR-T series setting file for IO-Link (IODD File)
This is the setting file to use when connecting the LR-T Series to an IO-Link master.
[LR-W Series] IO-Link Configuration file(IODD file)
This is the setting file to use when connecting the LR-W Series to an IO-Link master.
[LR-ZH] IO-Link Configuration File (IODD File)
This is the setting file to use when connecting the LR-ZH to an IO-Link master.
[FS-N40 Series] IO-Link Configuration File (IODD File)
This is the setting file to use when connecting the FS-N41C to an IO-Link master.
[FD-H] IO-Link Configuration File (IODD File)
This is the setting file to use when connecting the FD-H Series to an IO-Link master.
[FI-T] IO-Link Configuration File (IODD File)
This is the setting file to use when connecting the FI-T temperature sensor to an IO-Link master.
[FD-Q Series] IO-Link Configuration File (IODD File)
This is the setting file to use when connecting the FD-Q Series to an IO-Link master.
[FD-X Series] IO-Link Configuration File (IODD File)
This is the setting file to use when connecting the FD-X Series to an IO-Link master.
[FD-R Series] IO-Link Configuration File (IODD File)
This is the setting file to use when connecting the FD-R Series to an IO-Link master.
[FD-G Series] IO-Link Configuration File (IODD File)
This is the setting file to use when connecting the FD-G Series to an IO-Link master.
[GP-M Series] IO-Link Configuration File (IODD File)
This is the setting file to use when connecting the GP-MT to an IO-Link master.
[FL Series] IO-Link Configuration File (IODD File)
This is the setting file to use when connecting the FL Series to an IO-Link master.
[AI Series] IO-Link Configuration File (IODD File)
This is the setting file to use when connecting the AI Series to an IO-Link master.