Flow Sensor / Flow Meter Videos

Applicable models: FD-H / FD-Q / FD-R / FD-G / FD-EC / FD-EP / MP-F

Movies useful for using flow sensors / flow meters

FD-H Series

FD-H Installation

FD-H First Time Setup

FD-H User Calibration Guide

FD-Q Series

FD-Q Installation Tips

FD-R Series

Installation Support Videos

These videos will assist with the installation of the FD-R Series clamp-on flow meter.

FD-R Installation Tips

FD-R User Calibration Guide

Networking Support Videos

FD-R + MP-FEN1 Ethernet/IP Studio 5000 Setup and Messaging

FD-G Series

Installation Support Videos

These videos will help with the installation and setup of the FD-G Series.

FD-G First Time Setup Guide

FD-G 4-to-8-inch Installation Example

FD-G 1.25-to-3-inch Installation Example

FD-EC Series

Installation Support Videos

These videos will assist with the installation and use of the FD-EC Series clamp-on air flow sensor.

Installation

Cable Shortening

FD-EP Series

Installation Support Videos

These videos will assist with the installation and use of the FD-EP Series dual pressure and air flow sensor.

Installation

Cable Shortening

Installation of metal fittings (FD-EPB2)

Fitting installation (FD-EPB3)

MP-F Series

Installation Support Videos

These videos will assist with the installation and use of the MP-F Series air quality multi-sensor.

Drain cup installation

Main unit installation

Power monitor MP-FEA1 extension

CT installation

Networking Support Videos

MP-F + MP-FEN1 Ethernet/IP Studio 5000 Setup and Messaging

Product Lineup: