| 
                       1. Q: What is the communication cable for the Visual KV PLC to connect to your computer from both ports A and B (RJ-11 to 9 pin)? 
        A: OP- 26486 and OP-26487. 
         
        2. Q: Can we send and receive text out of both Visual KV serial communication  
        ports A and B? 
        A: We can receive text in and send text out of both communication ports. 
                      3. Q: What are the communication parameters for both serial ports A and B? 
        A: The communication parameters are 9600 baud rate, 8 bits, Even parity, and 1 stop bit. 
                      4. Q: How fast can I count incoming pulses into the new Visual KV series? 
        A: This series has two high speed counters rated at 30KHz, which means you can count a pulse every 33ms. 
                      5. Q: What is the maximum I/O I can have with the new Visual KV? 
        A: The maximum I/O I can have with the new Visual KV is 152. 
                      6. Q: What is the maximum amount of expansion units I can connect to one Visual KV PLC? 
        A: You can hook up 8 expansion units to one KV-16A/D(R/T) and KV-24A/D(R/T). You can only connect 7 expansion units to one KV-40A/D(R/T). 
                      7. Q: What are the high speed inputs rated at for the new Visual KV? 
        A: The input response time is decreased to 10ms whenever the HSP command is  
        used in the new Visual KV. 
                      8. Q: What is the fastest stepper motor output out of the new Visual KV? 
        A: The fastest stepper motor output is 50 KHz with the new Visual KV.  
                      9. Q: How many interrupts does the new Visual KV have? 
        A: There are 4 interrupts for the new Visual KV. 
        
                      10. What is the wiring diagram for the RS-232C communications cable? 
                      
                        
                          | RJ-11 connector | 
                           | 
                          9-pin connector | 
                         
                        
                          | Pin 3------ | 
                          --------- | 
                          Pin 3 | 
                         
                        
                          | Pin 4------ | 
                          --------- | 
                          Pin 5 | 
                         
                        
                          | Pin 5------ | 
                          --------- | 
                          Pin 2 | 
                         
                        
                           | 
                           | 
                          Pin 4 jumped to Pin 6 | 
                         
                        
                           | 
                           | 
                          Pin 7 jumped to Pin 8 | 
                         
                        
                           | 
                          OR | 
                           | 
                         
                        
                          | RJ-11 connector | 
                           | 
                          25-pin connector | 
                         
                        
                          | Pin 3------ | 
                          --------- | 
                          Pin 2 | 
                         
                        
                          | Pin 4------ | 
                          --------- | 
                          Pin 7 | 
                         
                        
                          | Pin 5------ | 
                          --------- | 
                          Pin 3 | 
                         
                        
                           | 
                           | 
                          Pin 4 jumped to Pin 5 | 
                         
                        
                           | 
                           | 
                          Pin 6 jumped to Pin 20 | 
                         
                        
                           | 
                           | 
                           | 
                         
                       
                      
                        
                      
                       
                     
  |