Introduction to Safety Standards
Risk Assesment
The Idea of Performance Level
Before Selecting Safety Equipment
Light Curtain Installation and Safety Distance (Minimum Distance)
Laser Scanner Installation and Safety Distance
  • Visualize / Robust / Easy Safety Light Curtain GL-V Series
  • Industry Leading Safety Laser Scanner Safety Laser Scanner SZ-V Series
  • Learn what safety measures to take: Safety Support Guidebook
  • Inquiry / Consultation Request

Light Curtain Installation and Safety Distance (Minimum Distance)

When installing a safety light curtain or other electrical detection protective device, refer to the minimum required distances for stopping the machine prior to the body reaching the hazardous zone when the body enters the detection zone. These distances are defined in standards such as ISO 13855. When installing a light curtain, be sure to provide the safety distance (minimum distance) determined by sources such as the standards, regulations, and laws of the country or area in which the light curtain will be used.

Calculating the Safety Distance according to ISO 13855

Safety distance (S) = Approach speed of the body × response time + additional distance (which varies depending on the detection capability of the sensor)

Perpendicular direction of approach

Detection of the body
S = K × T + C 40 < d ≤ 70
1.57" < d ≤ 2.76"
K = 1600 mm 62.99"/s (approach speed [assuming the walking speed of a person])
T = Maximum time required by the machine to stop + response time of the light curtain
C = 850 mm 33.46" (penetration distance [a value matching the standard length of a person’s arm])
Detection of fingers and hands
S=K × T + 8(d - 14) d ≤ 40
S = K × T + 8(d - 0.55") d ≤ 1.57"
K = 2000 mm 78.74"/s (approach speed [assuming the penetration speed of a hand])
T = Maximum time required by the machine to stop + response time of the light curtain
d = Detection capability of the light curtain

Note: If S is greater than or equal to 500 mm 19.69", perform the calculation again with K equal to 1600 62.99". If the newly calculated result gives S less than or equal to 500 mm 19.69", set S to 500 mm 19.69".

Relationship between the Maximum Time Required by the Machine to Stop and the Safety Distance

The value T shown in the formula is formed by adding the following two parameters. T = Maximum time required by the machine to stop + response time of the light curtain (ON → OFF)

When K (penetration speed) = 2000 mm 78.74"/s For example, when using the GL-R08H light curtain (which has a response time of 0.0069 s)
S = 2000 mm 78.74"/s × (maximum time required by the machine to stop + 0.0069 s) + C

As shown above, the maximum time required by the machine to stop is multiplied by the penetration speed (2000 mm 78.74"/s), so if the maximum time required by the machine to stop is increased by just 1 second, the safety distance is increased by (2000 mm 78.74"/s × 1 s = 2000 mm 78.74"). If the light curtain’s response time is increased by 1 ms, the safety distance is increased by 2 mm 0.08".

Basic Calculation Examples

Perpendicular direction of approach: GL-R Series

Formula:S = K × T + C
  • S: Minimum distance (mm inch; see the following figure) with S ≥ 100 mm 3.94"
  • K: Parameter extracted from the data based on the approach speed of the body (mm inch/s)
  • T: Overall system stop performance (s)
    T = t1 (GL-R Series maximum response time) + t2 (maximum time required by the machine to stop)
  • C:Penetration distance (mm inch)
    When d ≤ 40: 8 × (d - 14) with C ≥ 0
    When 40 < d ≤ 70: 850
    When d ≤ 1.57":8 × (d - 0.55") with C ≥ 0"
    When 1.57" < d ≤ 2.76": 33.46"
  • d: Detection capability of the GL-R Series (mm inch)
Calculation Example (1)-1
When using the GL-R60H
(detection capability d = 25 mm 0.98" and 60 beam axes)
Condition: Industrial application
K = 2000 mm 78.74"/s
t1 (GL-R60H response time) = 0.0157s
t2 (maximum time required by the machine to stop) = 0.1s
C = 8 × (25 - 14) = 88 mm 8 × (0.98" - 0.55") = 3.46"

S = K × T + C = 2000 ×(0.1157)+ 88 = 319.4mm
S = K × T + C = 78.74" × (0.1157) + 3.46" = 12.57"

If S is greater than 500 mm 19.69", perform the calculation again with K equal to 1600 mm 62.99"/s. If the newly calculated result gives S less than or equal to 500 19.69", set S to 500 19.69".
Calculation Example (1)-2
When using the GL-R08L
(detection capability d = 45 mm 1.77" and 8 beam axes)
Condition: Industrial application
K = 1600 mm 62.99"/s
t1 (GL-R08L response time) = 0.0069 s
t2 (maximum time required by the machine to stop) = 0.1 s
C = 850 mm 33.46"

S = K × T + C = 1600 × (0.1069) + 850 = 1021.04 mm
S = K × T + C = 62.99" × (0.1069) + 33.46" = 40.20"

Parallel direction of approach: GL-R Series

Formula:S = K × T + C
  • S: Minimum distance (see the following figure)
  • K: Parameter extracted from the data based on the approach speed of the body (mm inch/s)
  • T: Overall system stop performance (s)
    T = t1 (GL-R Series maximum response time) + t2 (maximum time required by the machine to stop)
  • C: Penetration distance (mm inch)
    C = 1200 - 0.4H with C ≥ 850 mm
    C = 47.24" - 0.4H with C ≥ 33.46"
    H: Height of the detection zone above the reference plane (mm inch)
    15 (d - 50) ≤ H ≤ 1000 with H ≥ 0
    (d - 1.97") ≤ H ≤ 39.37" with H ≥ 0"
Calculation Example (2)-1
When using the GL-R30L
(detection capability d = 45 mm 1.77" and 30 beam axes)
Condition: Industrial application
K = 1600 mm 62.99"/s
t1 (GL-R30L response time) = 0.0105 s
t2 (maximum time required by the machine to stop) = 0.1 s
H = 200 mm 7.87"
C = 1200 - 0.4 × 200 = 1120 mm
C = 47.24" - 0.4 × 7.87" = 44.09"
S = K × T + C = 1600 × (0.0105 + 0.1) + 1120 mm = 1296.8 mm
S = K × T + C = 62.99" × (0.0105 + 0.1) + 44.09" = 51.06"

Approaching the hazard by circumventing the top of the detection zone: GL-R Series

When it is not possible to prevent people from passing over the top of the detection zone in order to approach the hazardous zone, it is necessary to determine the height of the light curtain and the minimum distance S while keeping this issue in mind. You have to compare the S value calculated as shown below and the S value calculated under “Perpendicular Direction of Approach: GL-R Series” and set the larger value as the minimum distance S.

Formula:S = K × T + CRO
  • S: Minimum distance (mm inch; see the figure on the right) with S ≥ 100 mm 3.94"
  • K: Parameter extracted from the data based on the approach speed of the body (mm inch/s)
    K is determined according to the following table on the basis of S.
S (mm inch) K (mm inch/s)
100 ≤ S ≤ 500 3.94" ≤ S ≤ 19.69" 2000 78.74"
500 < S 19.69" < S 1600 62.99"

CRO is determined as shown in the following table according to the values a (height of the hazardous zone) and b (height of the top of the detection zone of the light curtain).

*1 Situations in which the height of the top of the detection zone is less than 900 mm 35.43" are not included because they cannot provide sufficient protection against circumvention and straddling.
*2 If the bottom of the detection zone is at a height of more than 300 mm 11.81" from the reference plane, sufficient protection cannot be provided against passing under the detection area to approach the hazard.

Calculation Example (3)-1
When using the GL-R60H
(detection capability d = 25 mm 0.98", 60 beam axes, and detection height of 1180 mm 46.46")
Condition: Industrial application
a (height of the hazardous zone) = 1400 mm 55.12"
b (height of the top of the detection zone of the light curtain) = 1180 + 300 = 1480 mm 46.46" + 11.81" = 58.27"
According to the above table, CRO is 850 mm 33.46".
(Because b is 1480 mm 58.27", it is between 1400 55.12" and 1600 62.99". In this situation, use a b value of 1400 55.12".)
  • K = 1600 mm 62.99"/s
  • t1 (GL-R60H response time) = 0.0157 s
  • t2 (maximum time required by the machine to stop) = 0.1 s
S = K × T + CRO = 1600 × (0.1157) + 850 = 1035.12 mm 62.99" × (0.1157) + 33.46" = 40.75"
(This is larger than the S value calculated under “Perpendicular Direction of Approach: GL-R Series.”)
Calculation Example (3)-2
When using the GL-R80H
(detection capability d = 25 mm 0.98", 80 beam axes, and detection height of 1580 mm 62.20")
Condition: Industrial application
a (height of the hazardous zone) = 1400 mm 55.12"
b (height of the top of the detection zone of the light curtain) = 1580 + 300 = 1880 mm 62.20" + 11.81" = 74.02"
According to the above table, CRO is 0 mm 0".
(Because b is 1880 mm 74.02", it is between 1800 70.87" and 2000 78.74". In this situation, use a b value of 1800 70.87".)
  • K = 2000 mm 78.74"/s
  • t1 (GL-R80H response time) = 0.0192 s
  • t2 (maximum time required by the machine to stop) = 0.1 s
S = K × T + CRO = 2000 × (0.1192) + 0 = 238.4 mm 78.74" × (0.1192) + 0" = 9.39"
(This is smaller than the S value calculated under “Perpendicular Direction of Approach: GL-R Series.”)
  • Visualize / Robust / Easy Safety Light Curtain GL-V Series
  • Industry Leading Safety Laser Scanner SZ-V Series

The page top