Coaxial Illumination

Optical Illumination Technique - Coaxial Lighting

Viewing highly-reflective objects with flat surfaces, such as ICs and cross-sectioned samples, is typically difficult to accomplish using ring illumination. When light hits the surface, most of it will reflect away from the lens and result in a dark image. Instead, coaxial (brightfield) illumination is used to view these targets and produce a bright image. Generally, this type of lighting makes use of a half-mirror to match the optical axes of the illumination and lens.

Schematic of light reflected from a specular surface

Light from an angle reflects away from the lens

Light from an angle reflects away from the lens
A : Lens B : Illumination C : Reflected light

Vertically illuminated light reflects to the lens

Vertically illuminated light reflects to the lens

A : Illumination B : Lens & CCD C : Specular reflection light
D : Half mirror (A half mirror reflects half of the light and transmits the rest) E : Mirrored surface

Schematic of coaxial illumination

Coaxial illumination image samples

Processed metal surface with ring illumination

Processed metal surface with ring illumination

Processed metal surface with coaxial illumination

Processed metal surface with coaxial illumination

IC with ring illumination

IC with ring illumination

IC with coaxial illumination

IC with coaxial illumination

We’re here to provide you with more details.
Reach out today!

Ask an Expert