Digital Microscopes
Inverted Microscopes
What is an inverted microscope?
An inverted microscope is a microscope with the objective lens placed below the stage on which the sample is located, allowing the sample to be observed from below.
This type of microscope is used for observation at higher magnifications than stereoscopic microscopes, with magnification ranging from about 20 to 1500x.
We’re here to provide you with more details.
Reach out today!

Structure of inverted microscopes
Inverted microscopes utilize an oblique light path leading to the eyepiece, allowing for observation in the same posture as a conventional microscope.
Because of the longer optical path, inverted microscopes use an optical system that relays the primary image from the objective lens to the eyepiece.
A : Light source B : Condenser lens C : Phase-contrast lens
D : Observation sample E : Objective lens F : Imaging lens
Path of light in an inverted microscope
We’re here to provide you with more details.
Reach out today!

Inverted microscope applications
Inverted microscopes are commonly used in the medical and biological fields, which require observation of cells in culture vessels (Petri dishes) from below.
In industrial fields, inverted microscopes are used to observe metallic materials, which can be easily fixed and focused on simply by placing the material with a polished surface facing downward.
The lack of an objective lens above the stage also makes it possible to observe large, heavy samples.
We’re here to provide you with more details.
Reach out today!

Weaknesses of inverted microscopes
- The observation distance is short.
- The shallow depth of field makes it difficult to observe targets with uneven surfaces.
- Capturing images requires an optional camera, but capturing high-resolution images is difficult.
- Microscopes are not equipped with measurement functions because the main purpose is observation.
We’re here to provide you with more details.
Reach out today!

Reasons for using a VHX Series digital microscope
The long observation distance and large depth of field makes it possible to observe with the entire image on the screen in focus whether at low or high magnification.
This eliminates the need to cut or polish the target. (Non-destructive observation is possible.)
Tilted observation of a connector (header)
5x
40x
Optical Shadow Effect mode and the 4K camera allow for high-resolution imaging.
Observation of tin-plated surface
2500x, normal image
Optical Shadow Effect Mode image
Observation of fractured surface (radial pattern)
40x, normal image
Optical Shadow Effect Mode image
The standard-equipped measuring microscope functions allow for measurement of planes and 3D profiles.
Graphite spheroidization rate measurement
100x, before measurement
After measurement
Connector profile measurement
50x, 3D image
3D measurement image
We’re here to provide you with more details.
Reach out today!