Digital Microscopes
Depth Composition
Basics of Digital Depth Composition
Even when the depth-of-field is shallow and the overall focus is poor, some areas of a target are still in-focus. As the distance between the lens and the object change, the area of focus also changes. By moving the lens throughout the different focal planes on a target, the VHX captures every pixel that comes into focus at each level and combines them into a single, fully-focused image.
A : Focus at the highest point B : Focus at the middle point
C : Focus at the lowest point
Extraction & composition
Real-Time Depth Composition
The advancement of depth composition technology also extends to processing speed in addition to image quality. No matter how brilliant a technique can be, it is not practical if the operation or calculation takes too long.
The high-speed processing technique of the VHX Series advances the technology to benefit users' analysis tools.
The real-time depth composition function allows you to display fully-focused images, in real-time, simply by moving the stage to the area of interest.
High-quality depth composition images can be generated in UXGA resolution with high-speed calculations and position/magnification correction.
Connector pins (50×)
Real-time depth composition & 3D display function
Capture the area of interest—no other operation required
You can quickly observe a depth composition image by just moving the motorized X-Y stage to view a desired area.
- Quick depth composition
- Faster observation and better analysis using more sample data
How depth composition works