Digital Microscopes
Coaxial Illumination
Optical Illumination Technique - Coaxial Lighting
Viewing highly-reflective objects with flat surfaces, such as ICs and cross-sectioned samples, is typically difficult to accomplish using ring illumination. When light hits the surface, most of it will reflect away from the lens and result in a dark image. Instead, coaxial (brightfield) illumination is used to view these targets and produce a bright image. Generally, this type of lighting makes use of a half-mirror to match the optical axes of the illumination and lens.
Schematic of light reflected from a specular surface
Light from an angle reflects away from the lens
A : Lens B : Illumination C : Reflected light
Vertically illuminated light reflects to the lens
A : Illumination B : Lens & CCD C : Specular reflection light
D : Half mirror (A half mirror reflects half of the light and transmits the rest) E : Mirrored surface
Schematic of coaxial illumination
Coaxial illumination image samples
Processed metal surface with ring illumination
Processed metal surface with coaxial illumination
IC with ring illumination
IC with coaxial illumination
We’re here to provide you with more details.
Reach out today!