Digital Microscopes
Observation and Measurement of Lenses Using Digital Microscopes
Lenses are widely used optical parts in daily life found in various products such as cameras, microscopes, telescopes, and glasses. Lenses are roughly divided into two types: convex lenses and concave lenses.
 
Optical lenses, such as telephoto lenses and zoom lenses, are created by combining multiple convex and concave lenses. This section explains the mechanism of lenses and introduces examples of their observation and measurement using digital microscopes.
What is Refractive Index?
 
A : Incident light B : Reflected light
C : Reflecting surface D : Refracted light
A refractive index is expressed with a value derived by dividing the speed of light in air by the speed of light in a substance.
As the speed of light varies according to the substance and the wavelength of light, the refractive index also varies according to the substance and wavelength of light. The direction in which light deflects can be calculated using Snell's law.
Snell's law (n1sinα = n2sinβ)
Refractive index 1 (e.g., air) : n1
Refractive index 2 (e.g., water, glass) : n2
Incident angle : α
Refraction angle : β
Get detailed information on our products by downloading our catalog.
View Catalog 
 
What is Dispersion?
 
A : White light
When white light passes through a prism, the spectrum of light appears.
This phenomenon is called the dispersion of light. It occurs because the refractive index differs according to the wavelength of light.
 
Note : nd is the refractive index of the D line emitted by sodium atoms.
The dispersion of an optical glass is expressed with a value called the Abbe number (v).
When dispersion is high
 
A : White light
With high dispersion, the spectral width of light increases.
When dispersion is low
 
A : White light
With low dispersion, the spectral width of light decreases.
We’re here to provide you with more details.
Reach out today!
 
Principle and Correction of Chromatic Aberration
 
A : Light beam B : Focal point
C : Differences in the focal distance
As shown in the following figure, the focal position of light with short wavelengths is close to the lens and that of light with long wavelengths is further away from the lens due to the dispersion of light. When light with a specific wavelength is brought into focus, light with other wavelengths becomes out of focus, which blurs the colors of the image. This phenomenon is known as chromatic aberration.
 
A : Light
What is spherical aberration?
Chromatic aberration occurs due to differences in the wavelengths of light. Aberration, however, occurs even with a single color, called monochromatic aberration. A typical example is spherical aberration. A convex lens surface is in the shape of part of a sphere. Therefore, the closer a point is to the edge of a lens, the larger the incident angle, which then increases the refraction angle. The phenomenon in which the focal position differs between points close to the lens center and points further away from the lens center is called spherical aberration.
 
A : Light
How to correct spherical aberration
Spherical aberration can be offset by, for example, combining a convex lens with a concave lens, which has aberration in the opposite direction, or combining lenses that have different refractive indices.
 
A : Light
Another method to offset spherical aberration is to use aspheric lenses. The spherical surface at the lens edge is processed to be a curved surface, instead of combining multiple lenses, which can correct the focal position without increasing the number of lenses.
We’re here to provide you with more details.
Reach out today!
 
Fluorite (Calcium Fluoride, CaF2) Lenses that Minimize Chromatic Aberration
Fluorite lenses, which are made from fluorite, are used when chromatic aberration needs to be minimized.
Made from natural fluorite, fluorite lenses have a low refractive index and low dispersion properties, which cannot be found in ordinary types of glass.
Additionally, fluorite lenses have low dispersion properties for wavelengths of light from red to green and extraordinary partial dispersion properties that greatly disperse wavelengths of light from green to blue. KEYENCE’s digital microscopes use fluorite lenses, so they provide excellent images with low aberration.
Normal glass
 
A : Red B : Green C : Blue
Fluorite
 
We’re here to provide you with more details.
Reach out today!
 
Observation and Measurement Examples of Lenses Using Digital Microscopes
These are the latest examples of observation and measurement of lenses using KEYENCE’s VHX Series 4K Digital Microscope.
Observation of a lens surface
The HDR function visualizes flaws and foreign particles on lens surfaces without using a scanning electron microscope (SEM).
 
ZS-200, 1500×, coaxial illumination + HDR
2D image
 
ZS-200, 1500×, coaxial illumination + HDR
3D profile measurement image
Observation of foreign particles in a sunglass lens
 
VHX-E200, 30×, ring partial illumination, before measurement
 
VHX-E200, 30×, ring partial illumination, automatic area measurement image
Observation of a sunglass lens with transmitted polarized illumination
 
VH-Z20, 30×, backlight + polarizing filter
Observation with transmitted polarized illumination visualizes residual stress, foreign particles, and cracks.
Observation of a lens surface
 
VH-Z20, 100×, ring illumination
Defective areas can now be captured.
Observation of flaws on a lens surface
 
VHX-E500, 500×
Coaxial illumination + Optical Shadow Effect Mode
Observation of flaws on a lens surface
 
ZS-20, 100×
Ring illumination + Optical Shadow Effect Mode
Optical Shadow Effect Mode can visualize flaws that used to be observed using a SEM.
Get detailed information on our products by downloading our catalog.
View Catalog