MONITOR MOTION
WITH PRECISION

  • Built in tools for displacement, velocity, and acceleration
  • Highest accuracy in its class
  • 392kHz sampling rate

Download Catalog

LK-G5000 Laser Displacement Sensor
  • How does the sensor work?

    The LK-G5000 is a laser triangulation sensor that calculates distance to its target using a CMOS chip and a known angle.

    What types of targets can be measured?

    The sensor uses advanced optics to get stable readings from virtually any surface including rubber, metal, and transparent targets.

    • Position monitoring

    • Glass vibration

    • Disc-rotor run-out

  • Why is sampling speed important?

    Sampling speed is a critical component for accurately capturing a target’s motion.

    Slower Sampling / 200μs sampling *Vibration cannot be measured. 50μs sampling *Vibration around the peak is not accurately measured. 5μs sampling / Faster Sampling

    When measuring a part vibrating at 2kHz, more data points can be collected per cycle at higher sampling speeds. This results in a more accurate curve.

SAME DAY SHIPPING DIRECT SUPPORT DIRECT SALES

WHY KEYENCE?

KEYENCE has been an industry leader in sensing technology since 1974. KEYENCE's direct sales team visits customers with live demo equipment to find the best possible solution for all applications.